Search Generac

Looking for Answers about Generac Power Systems 14kW Whole House Switch?

Business Standby(Q:31 A:33)
Centurion Series(Q:602 A:682)
CorePower Series(Q:188 A:210)
EcoGen(Q:79 A:94)
GP Series(Q:971 A:1139)
Guardian Series(Q:1665 A:1892)
Home Backup(Q:95 A:90)
HomeLink(Q:6 A:6)
LP Series(Q:174 A:181)
Parts & Accessories(Q:46 A:61)
PowerPact Series(Q:30 A:30)
Professional Grade(Q:27 A:30)
Protector Series(Q:32 A:37)
RS Series(Q:42 A:46)
Residential Grade(Q:253 A:288)
Synergy(Q:23 A:25)
Water Pumps(Q:10 A:11)
XD Series(Q:7 A:9)
XG Series(Q:389 A:420)
XP Series(Q:224 A:240)
iQ Series(Q:39 A:47)
iX Series(Q:121 A:203)
Shop now at Generac
or
Choose a Category
Most Recent Questions
Recent Question:
Where and what kind of key does the enclosure use?
Recent Question:
What size and type of engine is used? (cc, hp Numbers please)
Recent Question:
Pls remind me how to determine how many hours unit has run.
Recent Question:
6055 Generator alarm connections
Questions with Most Recent Answers
Question:
Model 6551 22KW - Cold Weather Kit
Question:
Can I extend the exhaust outlet to meet code for distance from windows or other opening?
Question:
Where do I find the error code meanings?
Question:
I need a wiring diagram to terminate my new #6437 in the main panel
Question:
how long can a whole house gernerac gen. run for

Customer questions and answers for
Generac Power Systems 14kW Whole House Switch

Back up much of your home—including a 4 ton central air conditioner—as well as a home office, garage, or additional rooms in your house.
Customer questions and answers:
240 Questions
 | 
256 Answers
Overall rating:
4.838 out of 5
4.8
out of
5

Customer questions and answers for Generac Power Systems 14kW Whole House Switch

Question

How does the 14KW generator handle short duration outages, ie a few seconds

State: NJ - New Jersey
Age: 55-64
This product will backup: Entire Home
asked 3 years, 7 months ago
Customer avatar
by
Stu
West Milford
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
The 14kW automatic standby generator has a start up delay; once utility power is lost, the generator will wait 10 seconds before starting. If utility power returns during this 10 second delay, the generator will not start. If the utility power has not returned during this 10 second delay, the generator will start and transfer, providing power to your home until utility power does return.
answered 3 years, 7 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
answer 2
If the outage is only for a few seconds, the control board would not as the generator to start.
State: MA - Massachusetts
Age: 45-54
This product will backup: Furnace
answered 3 years, 7 months ago
Customer avatar
by
NortheastTractor
Norfolk
0points
0out of 0found this answer helpful.
Question

How far away may I place this unit from my home?

I would like to install this unit about 100ft away from my home. I will have rigid conduit installed in the ground between the generator and the transfer switch.
Is this type of installation possible?
I will also plan on ordering the accessory remote display for convenience.
State: IL - Illinois
Age: 45-54
This product will backup: Entire Home
asked 4 years, 11 months ago
Customer avatar
by
Stan
chicago
on 14kW Whole House Switch
+4points
4out of 4found this question helpful.
Answer this question
3 answers
Answers
answer 1
You can install it that far away, but you will need to make a voltage drop calculation on your supply wire. Your wire size will increase due to the distance, which will also affect your conduit size.
This product will backup: Entire Home
answered 4 years, 11 months ago
Customer avatar
by
USAFPride
+1point
1out of 1found this answer helpful.
answer 2
It is possible to place the unit about 100 feet away from your home. However, we recommend installing the generator as close as possible to the transfer switch and fuel supply to reduce the length of piping needed. Laws and codes may regulate the distance and location of your installation.

For more detailed information, please contact an authorized Generac dealer near you by using our dealer locator at http://www.generac.com/Service/Deal...
State: WI - Wisconsin
answered 4 years, 11 months ago
Customer avatar
by
Generac
Waukesha
+1point
1out of 1found this answer helpful.
answer 3
The limit of distance is your budget for wire and depending on the placement of fuel source, the piping. At 100 feet between the Gen-Set and the Transfer Switch / Panel, I would recommend #4 copper wire type THHN in PVC conduit, or #4 copper wire type USE in direct burial. The #4 AWG wire is recommended to minimize voltage drop and to minimize amperage draw of motorized equipment. The advantage of installing conduit is that it does not need to be burried as deep and the control circuit wiring can be placed in the same conduit as the power wiring. Please verify wire sizing and grounding requirements of your local authority having jurisdiction. If utilizing natural gas, in order to minimize the pipe size, I suggest that you contact your local utility company and see if they will provide a 2 PSI source and place a regulator at the Gen-Set. If operating on Propane, either place the Tank in the vicinity of the Gen-Set, per local code, or run a medium pressure source to the Gen-Set and then place the low pressure regulator at the Gen-Set. Remember that in either case the Regulator Vent must be piped away from the Gen-Set for safety reasons. Remember to follow the recommended break-in procedure and to install the proper Engine Oil upon completion of the break-in period. Emergency use is not a substitute for proper break-in! Good Luck with your installation.
State: MD - Maryland
Age: 45-54
answered 4 years, 11 months ago
Customer avatar
by
Doug
+1point
1out of 1found this answer helpful.
Question

where can i get an owners manual for my guardian 14kw? its not online

 
Products related to my question
 
asked 3 years, 8 months ago
Customer avatar
by
LD
on 14kW Whole House Switch
+1point
1out of 1found this question helpful.
Answer this question
3 answers
Answers
answer 1
You can find a copy of the owner’s manual online by searching the model or serial number of the unit here: http://www.generac.com/Service/Manu.... If you are still experiencing difficulties locating a copy of your owner's manual online, please call us directly at 888-GENERAC (436-3722).
answered 3 years, 8 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
answer 2
The above answer is the spec sheet. I found my manual on:

http://www.generac.com/genApps/Libraries/Manuals/ViewManual.aspx?ItemNbr=0J7632&modelnbr=0058721
State: MD - Maryland
Age: 55-64
This product will backup: Other
answered 3 years, 8 months ago
Customer avatar
by
Cdwheels3
Silver Spring
+1point
1out of 1found this answer helpful.
answer 3
If a model 5872:

http://www.generac.com/SpecSheets/0186140SBY.pdf
State: MD - Maryland
Age: 55-64
This product will backup: Other
answered 3 years, 8 months ago
Customer avatar
by
Cdwheels3
Silver Spring
0points
0out of 0found this answer helpful.
Question

How close to the house can I install my 14 Kw gen.?

State: WI - Wisconsin
Age: Over 65
This product will backup: Entire Home
asked 4 years, 11 months ago
Customer avatar
by
tg
Milton,
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
Check out NFPA 37
State: NY - New York
Age: 45-54
This product will backup: Entire Home
answered 4 years ago
Customer avatar
by
Anonymous
Western NY
+1point
1out of 1found this answer helpful.
answer 2
Consult your local electrical codes for a final decision. However, Generac backup generators from 8 to 20kW can be installed as close as 18" from the home, if your local codes allow.
State: WI - Wisconsin
answered 4 years, 11 months ago
Customer avatar
by
Generac
Waukesha
+1point
1out of 1found this answer helpful.
Question

My propane company says I need 2 100 gallon tanks for a 14kw generator. I think 1 is sufficient to run it. Which is correct?

State: CT - Connecticut
Age: 55-64
This product will backup: Entire Home
asked 4 years, 7 months ago
Customer avatar
by
Michael
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
We used to install generators with one tank and found that in some cases a "vaporization" process occurred which stop the generator from running. The LP gas company we use found that using 2 tanks helped to resolve the problem. As a normal practice we now install 2 tanks when we have LP applications
State: MA - Massachusetts
Age: 55-64
answered 4 years, 6 months ago
Customer avatar
by
Christmasman
Methuen MA
+3points
3out of 3found this answer helpful.
answer 2
The answer depends upon how long you would like the generator to run continuously in a power outage. The 14kW Guardian Series consumes 2.30 gal/hr of liquid propane at full load. At that rate, you will have a little over 43 hours of continuous running time before your are out of fuel. You should size your propane fuel supply based upon how long you would want the generator to run in a power outage.

The only running requirements regarding LP fuel are regarding fuel pressure. At the generator inlet, fuel pressure must be 10 - 12" of water column for the generator to operate properly.

For additional fuel consumption information, please see the product spec sheet at http://www.generac.com/SpecSheets/0...
answered 4 years, 7 months ago
Customer avatar
by
GeneracPowerSystems
0points
0out of 0found this answer helpful.
Question

Generator mounting

Can I mount the 14KW generator on a pressure treated wood deck instead of a concrete pad? I was going to build a deck 8-10" off the ground to support the generator. Is this acceptable?
State: NY - New York
Age: 35-44
This product will backup: Entire Home
asked 4 years, 7 months ago
Customer avatar
by
JasonNY
NY
on 14kW Whole House Switch
+2points
2out of 2found this question helpful.
Answer this question
2 answers
Answers
answer 1
I would not recommend you do that. First the vibration and noise level will be more intence. Second your local building code may not allow you to do so. I would suggest that you build a 3' x 5' 2"x4" PT appron. Lay landscaping fabric on the bottom and fill with 3/4" crushed stone. This will reduce vibration and noise.
State: MA - Massachusetts
Age: 55-64
answered 4 years, 6 months ago
Customer avatar
by
Christmasman
Methuen MA
+1point
1out of 1found this answer helpful.
answer 2
Generac does not recommend mounting the generator on a combustible surface of any kind. Additionally, there might be local building codes that preclude such an installation.
answered 4 years, 7 months ago
Customer avatar
by
GeneracPowerSystems
+1point
1out of 1found this answer helpful.
Question

Is there a minimum distance from a natural gas regulator that this can be located?

State: NJ - New Jersey
This product will backup: Entire Home
asked 4 years, 7 months ago
Customer avatar
by
Kevin
on 14kW Whole House Switch
+1point
1out of 1found this question helpful.
Answer this question
2 answers
Answers
answer 1
If you had an LP tank the distance must be 10' away. Most building codes say NG service entrance must be 5' away from the generator. Check with your local codes.
State: MA - Massachusetts
Age: 55-64
answered 4 years, 6 months ago
Customer avatar
by
Christmasman
Methuen MA
0points
0out of 0found this answer helpful.
answer 2
Local codes usually dictates 5 - 10' from the point of ignition. To comply with your local codes, we recommend discussing with your local building code authority.
answered 4 years, 7 months ago
Customer avatar
by
GeneracPowerSystems
0points
0out of 0found this answer helpful.
Question

How loud is the 14K when operating compared to the portable version?

How loud is the unit, both when doing the weekly maintanance as well as when running at full load?
State: MA - Massachusetts
asked 4 years, 6 months ago
Customer avatar
by
Shawn
MA
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
66 db. 68 db respectively
State: MA - Massachusetts
Age: 55-64
answered 4 years, 6 months ago
Customer avatar
by
Christmasman
Methuen MA
0points
0out of 0found this answer helpful.
answer 2
The 14kW is 66dB under normal load and during the weekly self-test cycle. At this sound level, you can stil carry on a conversation while standing near the unit. In comparison, a portable generator will be louder.
answered 4 years, 6 months ago
Customer avatar
by
Generac1
0points
0out of 0found this answer helpful.
Question

I ordered the 14KW in early November and still have not received it. When can I expect to receive it? I live in NE Wisconnsin.

State: WI - Wisconsin
Age: Over 65
This product will backup: Entire Home
asked 4 years, 6 months ago
Customer avatar
by
Chilly
Door County WI
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
Lead times on the 14kw show 10-12 weeks but are subject to change.
State: MA - Massachusetts
Age: 45-54
This product will backup: Furnace
answered 4 years, 5 months ago
Customer avatar
by
NortheastTractor
Norfolk
0points
0out of 0found this answer helpful.
answer 2
I'm a contractor in NE and have 22 machines I ordered in early Nov. the ship date I got from Generac was 1/30 - 2/15.
State: MA - Massachusetts
Age: 55-64
answered 4 years, 6 months ago
Customer avatar
by
Christmasman
Methuen MA
0points
0out of 0found this answer helpful.
Question

Can I use an existinting natural gas line to connect and power my generator?

I already have a natural gas line that runs from my basement underground out to the back yard of my home. This line was previously used for a gas grill. I would like to use this line as the power source for my generator. Is that OK?

I am interested in either the Guardian 10KW or 14KW unit.
State: MD - Maryland
Age: 45-54
This product will backup: Entire Home
asked 4 years, 5 months ago
Customer avatar
by
Pwr2Brwnz
Baltimore
on 14kW Whole House Switch
+4points
4out of 4found this question helpful.
Answer this question
2 answers
Answers
answer 1
Most gas grills use less fuel than an automatic generator, so the existing line may not be sufficient. The gas line should be sized by a Generac dealer or a certified plumber, based on the volume and pressure required. For volume at full load, the 10kw requires 156,000 BTU/hr, and 220,000 BTU/hr for the 14kw. The pressure needed for both units is 5-7 inches of water column.
answered 4 years, 5 months ago
Customer avatar
by
GeneracPowerSystems
GeneracPowerSystems
0points
0out of 0found this answer helpful.
answer 2
You will need to have a local plumber check the line for leaks and to make sure it is of the proper size BEFORE attempting to connect the unit. You will also need to make sure the line complies with all current codes in your area.
State: MA - Massachusetts
Age: 45-54
This product will backup: Furnace
answered 4 years, 5 months ago
Customer avatar
by
NortheastTractor
Norfolk
-1point
0out of 1found this answer helpful.
Question

does a 120 liter tank fit generacs 14kv?

im planning on buying one generac 14 kv for my home but i do not have a direct gas line on my home, my dealer says it can run with a 120 liter tank next to it but im wondering how long a 120 liter natural gas can last until it runs out of gas? thanks in advance!
Age: 25-34
This product will backup: Entire Home
asked 4 years, 1 month ago
Customer avatar
by
jojo
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
The smallest propane tank we can recommend for use with our current 2013 and newer automatic standby generators that utilize an Evolution Controller is a 250 gallon tank. The answer above is referring to the 2010 Nexus Controller product only. The volume and pressure required for the unit can be located in the owner’s manual and installation guidelines that are provided with the unit. The fuel consumption for each model number can vary, and we recommend ensuring the documentation utilized reflects your particular generator’s model number. To locate a copy of the owner’s manual and installation guidelines for your particular unit, search the model or serial number here: http://www.generac.com/Service/Manu....
answered 3 years, 2 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
answer 2
The 14kW automatic standby generator is designed to be run off of natural gas supplied by a utility line, or propane supplied by tank. The smallest propane tank a unit can run off of is 120 gallons. Natural gas is not able to be compressed in the same manner that propane is, so running off of a natural gas tank is not recommended. The volume and pressure required for the 14kW unit utilizing natural gas is 220,000 BTU/hr with 5-7” of water column, and if utilizing propane is 211,680 with 10-12” of water column.
answered 4 years, 1 month ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
Question

Can Guardian 14kw unit be bolted to the concrete pad?

We are worried about earthquakes and theft. Is there a way to bolt the unit down? If so, please provide us with the distances between the holes underneath the unit so that we can ask our contractor to pour the concrete according to spec. Thanks.
State: CA - California
Age: 45-54
This product will backup: Other
asked 3 years, 10 months ago
Customer avatar
by
Wind
Groveland
on 14kW Whole House Switch
+1point
1out of 1found this question helpful.
Answer this question
2 answers
Answers
answer 1
The 14kW automatic standby unit can be mounted to a concrete pad using the 1 3/16 ” diameter bolt holes in the interior of the enclosure. A diagram of the hole locations is included in your owner’s manual under the Installation Diagrams section. When the unit is delivered, there will be bolts already occupying those spaces, as that is how the composite mounting pad is connected to the base of the generator. You would remove the existing bolts in order to properly anchor the generator and composite mounting pad to your concrete pad. The bolt diameter should equal that of the existing bolts, and should be a height of approximately three inches; however, the distance as to which the bolts are sunk into the concrete would be determined either by your local inspector if mounting is required by local code, or by your installer to ensure that the unit is properly anchored.
answered 3 years, 9 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
answer 2
Yes, Generac partners with a company called diversitech which sells "genpads" which have pre drilled/threaded holes inside which will mate to your generator to allow it to be bolted down creating a more secure installation.
State: NY - New York
answered 3 years, 9 months ago
Customer avatar
by
Mark
Long Island
0points
0out of 0found this answer helpful.
Question

How many hours does the generator last if it has a 100 pound propane gas tank

This product will backup: Entire Home
asked 3 years, 9 months ago
Customer avatar
by
JDD
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
The smallest propane tank we can recommend for use with our current 2013 and newer automatic standby generators that utilize an Evolution Controller is a 250 gallon tank. The answer above is referring to the 2010 Nexus Controller product only. The volume and pressure required for the unit can be located in the owner’s manual and installation guidelines that are provided with the unit. The fuel consumption for each model number can vary, and we recommend ensuring the documentation utilized reflects your particular generator’s model number. To locate a copy of the owner’s manual and installation guidelines for your particular unit, search the model or serial number here: http://www.generac.com/Service/Manu....
answered 3 years, 2 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
answer 2
The smallest propane tank we can recommend is a 120 gallon tank. The volume and pressure required for the 14kW unit utilizing liquid propane is 211,680 BTU/hr with 10-12” of water column. The 14kW unit will consume approximately 2.3 gallons per hour when operating at full load.
answered 3 years, 9 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
Question

When the unit kicks in due to power outage Is it recommended to run the unit continuously or should I shut down for a period time ?

State: CT - Connecticut
Age: 45-54
This product will backup: Entire Home
asked 3 years, 8 months ago
Customer avatar
by
Tony
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
We recommend shutting the unit down after every 24 hours of operation to check oil levels and other maintenance items, such as the air filter. This will help make certain that the unit will continue without flaw when called upon to run for an extended period of time. After these maintenance items have been checked, the unit can be restarted. You can find further information regarding 24 hour shut down in the Checking the Engine Oil Level section of the owner’s manual that is provided with the unit.
answered 3 years, 8 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
answer 2
You should stop it every 24 hours to inspect the oil level
State: NY - New York
answered 3 years, 8 months ago
Customer avatar
by
Mark
Long Island
0points
0out of 0found this answer helpful.
Question

How long will the unit run @50% load on 1, 100 gal. propane tank?

State: NY - New York
Age: 55-64
This product will backup: Entire Home
asked 3 years, 8 months ago
Customer avatar
by
frank
Salt point
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
The smallest propane tank we can recommend for use with our current 2013 and newer automatic standby generators that utilize an Evolution Controller is a 250 gallon tank. The answer above is referring to the 2010 Nexus Controller product only. The volume and pressure required for the unit can be located in the owner’s manual and installation guidelines that are provided with the unit. The fuel consumption for each model number can vary, and we recommend ensuring the documentation utilized reflects your particular generator’s model number. To locate a copy of the owner’s manual and installation guidelines for your particular unit, search the model or serial number here: http://www.generac.com/Service/Manu....
answered 3 years, 2 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
answer 2
The smallest propane tank we can recommend is a 120 gallon tank. The volume and pressure required for the 14kW unit utilizing liquid propane is 211,680 BTU/hr with 10-12” of water column. The 14kW unit will consume approximately 2.3 gallons per hour when operating at full load, and will consume approximately 1.56 gallons per hour when operating at half load.
answered 3 years, 8 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
Question

While the generator is running do you recommend limiting power usage in the home or does it make little difference (as long as you are not exceeding t

...as long as you are not exceeding he power capacity of the generator.
State: PA - Pennsylvania
Age: 35-44
asked 3 years, 8 months ago
Customer avatar
by
Tjh
Pa
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
If you are on propane you should try to economize your usage to burn less fuel... Which can be difficult to restock in an emergency.... If on natural gas you still economize to not over stress unit. Treat it as you would any engine which is to say not to run it to its highest rpm and stress all the time if you want to minimize wear and tear
State: NY - New York
answered 3 years, 8 months ago
Customer avatar
by
Mark
Long Island
0points
0out of 0found this answer helpful.
answer 2
The 14kW unit can cover a wide range of household appliances and items, however the exact items it can cover will vary for each application. The 14kW automatic standby generator is rated for a continuous output of 14,000 watts when utilizing propane, with a rated amperage of 58.3 amps at 240 volts. When utilizing natural gas, the unit is rated for a continuous output of 13,000 watts, with a rated amperage of 54.2 amps at 240 volts. You will want to ensure that all of the items you intend to run will not exceed this rating.
answered 3 years, 8 months ago
Customer avatar
by
GeneracPowerSystems01
0points
0out of 0found this answer helpful.
Question

DOES NATURAL GAS PROVIDE MORE POWER THEN PROPANE

IS THERE LESS POWER OUTPUT WITH NATURAL GAS THEN PROPANE?
State: NY - New York
Age: 55-64
asked 1 year, 11 months ago
Customer avatar
by
ROBERT
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
2 answers
Answers
answer 1
Yes, there is less BTU in an equal amount NG than propane. Generac notes that, a 14 kw unit propane has only 13 kw with NG.
State: NH - New Hampshire
Age: 55-64
answered 9 months ago
Customer avatar
by
Rick
Windham
0points
0out of 0found this answer helpful.
answer 2
Generac’s 14kw Guardian Series automatic standby generators, will not differentiate in power output, when utilizing either a natural gas or liquid propane vapor fuel source. Either of these sources will help the unit take on a continuous power capacity of 14,000 watts, and a maximum continuous load current of 58.3 amps at 240v. Further product specifications can be located online, by using your product’s model or serial number via the following link: http://www.generac.com/service-supp....
answered 1 year, 11 months ago
Customer avatar
by
GeneracPowerSystems02
0points
0out of 0found this answer helpful.
Question

Is there a way to change how long the generator runs in the excercise mode?

asked 4 years, 11 months ago
Customer avatar
by
kirk
on 14kW Whole House Switch
-2points
0out of 2found this question helpful.
Answer this question
1 answer
Answers
answer 1
No, you cannot change how long the exercise cycle runs, although you can change the day and time that it runs.
State: WI - Wisconsin
answered 4 years, 11 months ago
Customer avatar
by
Generac
Waukesha
+1point
1out of 1found this answer helpful.
Question

where can i find a switch (Manual, Off, On) in Connecticut

State: CT - Connecticut
Age: 35-44
This product will backup: Entire Home
asked 4 years, 10 months ago
Customer avatar
by
Greg
Norwich
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
1 answer
Answers
answer 1
We recommend using a Generac automatic transfer switch with the 14kW generator. To purchase the right switch for your application, find a dealer near you by using our dealer locator at http://www.generac.com/Service/Deal...
State: WI - Wisconsin
answered 4 years, 10 months ago
Customer avatar
by
Generac
Waukesha
0points
0out of 0found this answer helpful.
Question

Maintenance during extended power outage

Model 55221
During an extented power outage, what service checks should be performed and how frequently? How do you turn off the unit (allowing sufficient cool down) to perform this service? The operation manual does not explain how to perform these checks.
State: MA - Massachusetts
Age: 55-64
This product will backup: Entire Home
asked 4 years, 10 months ago
Customer avatar
by
Al G
Chelmsford
on 14kW Whole House Switch
0points
0out of 0found this question helpful.
Answer this question
1 answer
Answers
answer 1
We recommend stopping the unit and checking the oil after 24 hours of straight operation and changing the oil and oil filter after 200 hours of operation. It may be necessary to top off the oil during an extended outage since all air cooled engines do consume a minor amount of oil.

To begin this process, turn off the breaker on the generator to take the load off of it. Then turn the auto/off/manual switch on the control panel to the off position. Once this is complete, an oil change can be done if required.
State: WI - Wisconsin
answered 4 years, 10 months ago
Customer avatar
by
Generac
Waukesha
+1point
1out of 1found this answer helpful.
1 2 3 4 5 ... 12 next>>